Hi All,
I am in process of designing a custom BLE remote control based on TI CC2541. Before designing the hardware, I bought two dev kits from TI, CC2541DK-MINI and CC2541DK-RC to evaluate the performance and give something to the software team until the custom remote control design is finished.
The (embedded) PC I am trying to control runs a Linux CentOS 7.0 and incorporates an Intel Bluetooth module which supports BLE, hence I don't use/need the USB dongle. I successfully could communicate with the CC2541DK-MINI devkit using hcitools but it fails when I want to connect to the CC2541DK-RC.
I wonder if there is a simple way of communicating with the CC2541DK-RC. What I need to do is to capture events when a key is pressed on the remote control.
Thanks