I have recreated the TIDA-00096 design and am currently in the testing phase of the PCB and the firmware. I can successfully flash the firmware to CC2541, the communication with ADS1293 supposedly works as well, but I just cannot get the BLE to a working phase.
After some debugging and testing, I have found out, that if I flash SimpleBLEPeripheral, my PC will find, pair and connect with the target (TIDA-00096). However if I flash the firmware that is provided for TIDA-00096, PC and Android 4.1.2 based phone won't find any Bluetooth devices at all.
Android 6.0 phone will however now see the target by name "ADS1293 ECG Wireless Demo" and also ask for PIN (which is 000000 as far as I know), when I try to connect to it. It will then usually return error "Unable to communicate with ADS1293, please make sure that the device is ready to pair" error in the 1st/2nd try, but in the 3rd try, it will finally add it to "Paired devices" list, however it won't state "connected" status.
I was wondering what may be the cause for this and how to find a solution?