Hi,
I'm trying to run the SPPDemo example (on MSP430BT5190 microcontroller) with a cpu frequency of 25MHz. My hardware is an own PCB (equal to EZ430-RF256x reference design) with a MSP430BT5190 and one external 32.786kHz ±20ppm clock.
The cpu frequency are configured in the HRDWCFG.h-File. There is "cf8MHZ_t, cf16MHZ_t, cf20MHZ_t, cf25MHZ_t" selectable.
#define BT_CPU_FREQ (cf25MHZ_t)
I configured an unused pin as CLK-output and find out, that the cpu frequency is still 22.1184MHz not 25MHz. Why is this so? To configure an uart with an other microcontroller (MSP430 <-> STM32) I need the correct and exact frequency.
Software:
SPPDemo (CC256XMSPBTBLESW-v1.5-R2)
Hardware:
MSP430BT5190 with external 32.786kHz ±20ppm
PAN1326B (CC2564B) (dual supply voltage 3.3V and 1.8V)
Thank you!
Regards,
Constantin