Part Number: CC2541DK-SENSOR
Tool/software: TI C/C++ Compiler
I have got older project which was build ....... and now if I build same project on new Desktop system after installation of IAR 8.2 license version (dongle ) I get error stated above.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2541DK-SENSOR
Tool/software: TI C/C++ Compiler
I have got older project which was build ....... and now if I build same project on new Desktop system after installation of IAR 8.2 license version (dongle ) I get error stated above.
Hi Rachel,
I was busy with some other project, so I could not replay soon. After installation of perl,error solved but now I am stuck with new error provided below.
Fatal Error[e72]: Segment SLEEP_CODE must be defined in a segment definition option (-Z, -b or -P)
version I am currently have
IAR Embedded Workbench for 8051 IDE - Version 8.20.1
IAR Embedded Workbench common components -6.4.6.2419
Hello ,
Currently I have BLE SDK version 1.3.2 and IAR version 8.2. The source code I am building got from our one of client, they all ready builded project, help me out where I am wrong.
Thanks and Regards
Rafakath
Hi Mohammad,
Did your client use the same version of IAR that you are using? Do you get the same error if you import the default SensorTag project into your version of IAR?
Projects for BLE-Stack v1.3.2 were built and verified with IAR v8.10. Although you may be able to get your project working with IAR 8.20, I would recommend you update to at least BLE-Stack v1.4.0 which was built and tested with IAR 8.20. You can find the steps to port a project on our BLE wiki page: http://processors.wiki.ti.com/index.php/LPRF_BLE_Porting_Projects