Other Parts Discussed in Thread: CC256XMS432BTBLESW
Tool/software: Linux
We are using CCS v8 on MAC and Ubuntu for development. Our HW setup is MSP432P401R + CC2564MODA. How can we install the CC256x BT stack on MAC and Ubuntu??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
We are using CCS v8 on MAC and Ubuntu for development. Our HW setup is MSP432P401R + CC2564MODA. How can we install the CC256x BT stack on MAC and Ubuntu??
Basavaraj Hiremath said:How can we get the project working on non-Windows machines?
There is no easy way to install the SDK on a non-Windows machine. However, you can install the SDK on a Windows machine and then copy the content in the installation directory (typically : C:/ti/Connectivity/CC256X BT) to a non-Windows machine.
Depending on your IDE, you may or may not be able to build the sample applications on your non-Windows machine. You are welcome to try. But it is best to use Windows.
BR,
Vihang
Thanks Vihang,
I was able to build from MAC by copying the files. But now I am getting this error:
[Start: Texas Instruments XDS110 USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/Users/basuhire/.ti/ti/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'libjioxds110.dylib'.
The library build date was 'Feb 8 2018'.
The library build time was '18:21:48'.
The library package version is '7.0.188.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
[End: Texas Instruments XDS110 USB Debug Probe]