This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564: VS_Set_Bluetooth_Address v. GAP_Query_Local_BD_ADDR functions

Part Number: CC2564

BT Family & Friends,

Our customer is asking the following:   We are trying to use the vendor specific function VS_Set_Bluetooth_Address to set the board MAC address.  However, even though the return value from the function indicates that the function succeeded, when we check the board mac address using the GAP_Query_Local_BD_ADDR function, the MAC address is not changed.   What could be the problem? Thanks.

We've asked to verify with a Sniffer app on mobile device and indeed the MAC address is not changed.  There are also other function parameters to pay attention to such as frequency, etc but these should not impact whether or not the MAC address is indeed written or read to.  Thoughts?

TY,

CY