Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640,
Hi
I am trying to flash the CC2640R2 using UART but it is giving the error as attached in the image.
I am using a TIL-232R-3V3 cable for UART level translation
I have modified the CCFG file and configured BL pin as DIO 12. Below is the code snippet
//#####################################
// Bootloader settings
//#####################################
#ifndef SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE
//#define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE 0x00 // Disable ROM boot loader - Mahesh
#define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE 0xC5 // Enable ROM boot loader - Mahesh
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_LEVEL
#define SET_CCFG_BL_CONFIG_BL_LEVEL 0x0 // Active low to open boot loader backdoor - Mahesh
//#define SET_CCFG_BL_CONFIG_BL_LEVEL 0x1 // Active high to open boot loader backdoor - Mahesh
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_PIN_NUMBER
#define SET_CCFG_BL_CONFIG_BL_PIN_NUMBER 0x0C // DIO number for boot loader backdoor - Mahesh
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_ENABLE
#define SET_CCFG_BL_CONFIG_BL_ENABLE 0xC5 // Enabled boot loader backdoor - Mahesh
//#define SET_CCFG_BL_CONFIG_BL_ENABLE 0xFF // Disabled boot loader backdoor - Mahesh
#endif
Please let me know how if I have missed any steps for the same
Regards
Mahesh H M