Other Parts Discussed in Thread: ENERGYTRACE
Hi,
i want to use the UART Interface (Target Auxiliary Connector) on XDS110 Debug Probe for HCI tests on CC2640R2F but i get a connection Error on BTool Application.
When i do the same with the XDS100 OnBoard debugger the connection was working. But in future we want to use the XDS110 debug probe for production tests.
CC2640R2F Test Firmware: host_test_cc2640r2lp_app
Power at the DUT is 3.3V
Any idea what i'm doing wrong with the XDS110
BR
Claus