Part Number: CC2640R2F
Hi,
I tested the Rising supply-voltage slew rate on launch pad.
yes, with the power of Lauchpad (5V to 3.3V), it is about 56mV/us, it meets the requirement.
but, when I power the VDDS line (after the bead FL1) with Power supply (3V, not a battery), even with a 10uS cap after, it can reach about 3000/6.25uS= 480mV/us. it is definitely over the limit of spec.
if we assume there is no current limit or zero inner resistance of the power supply, the cap won't help to decrease the slew rate any more.
do you suggest other solution for this kind of power supply topology with high efficiency?
BR. Albin