Other Parts Discussed in Thread: CC256XB-BT-SP
Hello,
Regarding EN 300 328 v2.1.1, our product is classified as a receiver category 1 as the Max RF output power is greater than 10dBm eirp. (antenna gain +1.3dBm).
To complete our product certification process, we have to determine the adaptive mechanism in place in the CC2564MODN and establish a procedure to test them.
Could you please help me to answer the following questions as there are requested by our test house and are not clearly defined in the datasheet:
1- Which type of adaptive equipment is it ?
a- non-adaptive Equipment
b- adaptive Equipment without the possibility to switch to a non-adaptive mode
c- adaptive Equipment which can also operate in a non-adaptive mode
2- In case of adaptive equipment:
a- The maximum Channel Occupancy Time implemented by the equipment in ms ?
b- The equipment has implemented an LBT based DAA mechanism - yes/no ?
c- if different modulation from FHSS, the equipment is Frame Based equipment - yes/no ?
d- if different modulation from FHSS, the equipment is Load Based equipment - yes/no ?
e- if different modulation from FHSS, the equipment can switch dynamically between Frame Based and Load Based equipment - yes/no ?
f- The CCA time implemented by the equipment in µs ?
g-The equipment has implemented a non-LBT based DAA mechanism - yes/no ?
h- The equipment can operate in more than one adaptive mode - yes/no ?
i- The equipment has implemented Short Control Signalling Transmissions - yes/no ?
Thank you for your help,