Other Parts Discussed in Thread: CC2650, CC2540
Tool/software: TI-RTOS
Hello,
I have my CC2650 SensorTag.
CC2650 SensorTag has IR temperature sensor and I want the temperature data to be sent wirelessly to a computer. Then, I can read the data from Com Port and do some analysis using LabVIEW. I have to finish this task in wireless approach. I want the data to be read from com port because it is the easiest way for me to get the sensor data to LabVIEW for analysis.
I have one idea which is using CC2540 Usb dongle and I have it right now. However, I have no idea on how to achieve my task. I think that the temperature data from CC2650 SensorTag can be wirelessly transmitted to the CC2540 Usb dongle, once the usb receives the data, I can read the data through Com Port using Putty, is this possible? If so, how can I achieve this?
I have searched from the Internet but it seems that there is not a complete solution. I am a beginner in this field and therefore any suggestions for me will be much appreciated!!
Thanks for your help!