Hello,
We are using the advertisement extension feature of Bluetooth 5 using Host test application in cc2640R2F using Bluetooth 5 SDK where we are having following queries:
1) The advertisement extension feature allows for sending advertisement on any of 40 channels, what is method for this channel selection?
2) We are able to send advertisement extension in coded S2 or S8 mode but we are not able to send advertisement in 2 Mbps mode, what is probable reason for this?
3) BT 5 supports advertisement of length till 255 bytes, but we are able to successfully transfer only 200 bytes. If we send more than 200 bytes, the advertisement command response from HCI tester comes successful but on receiving launchpad, we are only able to receive 200 bytes, post that it fragment the packet. Why are we not able to receive packet more than 200 bytes.
Regards
Prateek