Other Parts Discussed in Thread: CC2650
I have connected CC2650 SimpleLink SensorTag to the Sensortag Android app. When I try to push data to to a ThingsBoard instance on my LAN, the app either crashes or restarts.
Steps to reproduce:
1) Start SensorTag device.
2) Start Android SensorTag app.
3) Choose the SensorTag device on the main screen
4) Press Advanced-button under "Cloud View"
5) Set up Cloud as follows:
a) Cloud service: Choose "Custom"
b) Username: Use access token from ThingsBoard
c) Password: Leave empty
d) DeviceID: Leave as is
e) Broker Address: Enter the LAN-address of ThingsBoard instance
f) Broker Port: Enter the port address of ThingsBoard instance
g) Publish Topic: Enter "v1/devices/me/telemetry"
h) Clean session: Enable
i) Use SSL: Enable
j) Press "Save"
6) Enable "Push to Cloud"
7) The app does not connect, but instead restarts or crashes.
Sensortag App Version: v,5,4,0 (Build 47)
CC2650 SimpleLink SensorTag details:
- Firmware rev.: 1.30
- Hardware rev.: PCB 1.2/1.3
Android device details:
- Type: Samsung Galaxy A7 (2018)
- Mod.nr.: SM-A750FN/DS
- Android v.: 9
- Kernel v.: 4.4.111-15516145