I have a board with a input button on P1_0.
How do I setup the proper code to enable interrupt on that port ?
I have tried to change the parameters on hal_key.c to reflect this but I have been unsuccessful.
Here is my setup for hal_key.c:
#define HAL_KEY_RISING_EDGE 0
#define HAL_KEY_FALLING_EDGE 1
#define HAL_KEY_DEBOUNCE_VALUE 25
/* CPU port interrupt */
#define HAL_KEY_CPU_PORT_1_IF P1IF
/* SW_1 is at P0.0 */
#define HAL_KEY_SW_1_PORT P1
#define HAL_KEY_SW_1_BIT BV(0)
#define HAL_KEY_SW_1_SEL P1SEL
#define HAL_KEY_SW_1_DIR P1DIR
#define HAL_KEY_SW_1_IEN IEN2 /* CPU interrupt mask register */
#define HAL_KEY_SW_1_ICTL P1IEN /* Port Interrupt Control register */
#define HAL_KEY_SW_1_ICTLBIT BV(0) /* P0IEN - P0.0 enable/disable bit */
#define HAL_KEY_SW_1_IENBIT BV(4) /* Mask bit for all of Port_0 */
#define HAL_KEY_SW_1_PXIFG P1IFG /* Interrupt flag at source */
#define HAL_KEY_SW_1_EDGEBIT BV(0)
Thanks
Christian