Other Parts Discussed in Thread: CC2640
Hi,
I just noticed that in the post below Clément has mentioned:
"on CC2640, the RTLS is based on BLE 3. If you want RTLS based on BLE 5, then you need to migrate to CC2642 / CC2652"
https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/538/t/852440?tisearch=e2e-sitesearch&keymatch=Angle%2520of%2520Arrival
Could you please shed some lights on the following questions :
1. Have you implemented the AoA direction-finding capability in the BLE 5 stack at all? (Even for CC2642 / CC2652) If yes which example in which SDK covers that?
2. Can implementation of AoA direction-finding capability on the BLE 5 stack lead to higher precision or better results with respect to using BLE 3? If yes, why?
3. Except for the precision in the question above, what are there the other possible differences? (for example how the range is different? )
4. Why 3 devices have used to implements the AoA example instead of 2? Can't it still be implemented on the BLE 3 with just 2 devices?
Thanks
Regards