Other Parts Discussed in Thread: CC2640, CC2642R-Q1, , CC2642R, CC2640R2F
Dear Experts,
could You please let me know, what the best way is to distinguish between CC2640R2F-Q1 and CC2642R-Q1 devices. Basically we would have CC2640 and CC2642 based HW and would like to distinguish those in SW.
I checked the TRM and there are different instances of information, which could be potentially the right approach, but it is not 100% clear from the register definitions.
As far as I can see following registers could be used
1) SHDW_DIE_ID_0, SHDW_DIE_ID_1, SHDW_DIE_ID_2, SHDW_DIE_ID_3 --> could not find interpretation of those registers
2) USER_ID & FCFG1:ICEPICK_DEVICE_ID --> Is it possible to unambiguously distinguish between CC2640R2F and CC2642R devices using those registers and how?
Thanks and best regards,
Gregor