Greetings, TI,
I would like to build my own physical-layer driver accessing basic-rate bluetooth packets. I'm basing my prior knowledge on the CC2400 transceiver, which is apparently deprecated. However, this part has features that I'm looking for: register-level transceiver physical layer control. I'd like to ask what might be the recommended TI migration path? And if you can recommend such a part, would there be an integrated processor/radio eval board for it?
Summary of what I'd like:
(1.) supports basic-rate bluetooth physical layer (1 MHz channels, 1 Mbps baudrate, GFSK). NOT BLE or Zigbee, thanks.
(2.) direct radio control like the CC2400 via register r/w, perhaps fifo/spi output or any equivalent.
(3.) NOT a high-level black-box interface like Bluetopia/CC2564x.
Thank you!