Other Parts Discussed in Thread: CC2650STK, BLE-STACK
Tool/software: Code Composer Studio
Simple Goal: We wish to compile Out-of-Box example for CC2650STK SensorTag, for purposes of displaying interface with iOS app.
Fresh install of CCS 10.1 on Windows 10
BLE-STACK 2.02.05.02
Some snippets from build log:
...
Build of libraries done.
clem3 package/cfg/app_ble_pem3.c ...
"package/cfg/app_ble_pem3.c", line 8290: warning #112-D: statement is unreachable
"package/cfg/app_ble_pem3.c", line 8808: warning #112-D: statement is unreachable
"package/cfg/app_ble_pem3.c", line 8988: warning #112-D: statement is unreachable
...
warning #10229-D: output section ".data" refers to load symbol "user0Cfg" and hence cannot be compressed; compression "lzss" is ignored
undefined first referenced
symbol in file
--------- ----------------
user0Cfg <whole-program>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "sensortag_cc2650stk_app.out" not built
>> Compilation failure
makefile:229: recipe for target 'sensortag_cc2650stk_app.out' failed
gmake[1]: *** [sensortag_cc2650stk_app.out] Error 1
makefile:225: recipe for target 'all' failed
gmake: *** [all] Error 2
Other warnings include:
#10229-D output section ".data" refers to load symbol "user0Cfg" and hence cannot be compressed; compression "lzss" is ignored
This project was created using a version of compiler that is not currently installed - 16.9.4.LTS [ARM]. -- which I cannot readily find in Software Updates area... (my suspicion is that this is the least of the problems.)
(The sensortag...stack project builds AOK.)
(compile log attached)