Hello,
I'm trying to print some float values on my project. My application is based on Project Zero example that uses Log_Info to print via UART. I already searched for related questions on this forum and added this line to app_ble.cfg as stated by some people that it worked for them:
System.extendedFormats = "%f";
But that didn't work as all I get when I try to print my value is "0.0000" for a value that should be between 0.25 and 0.5.
This is the line that prints the float value:
Log_info1("roll = %f", roll);
And roll was declared as a float type.
I know that is unadvised to use floats but this time is a must.
Best regards and thanks.