Part Number: CC2564MODN
Other Parts Discussed in Thread: CC2564, CC2650
Hello,
I am working on a project in which we are looking to use the CC2564MODN module with integrated antenna. I want to make sure that I have all of the hardware necessary to code and develop this board. Some software engineers will be working on the code but need to make sure that they have all the resources to do so.
Is there anything else needed besides the Evaluation board: CC2564MODAEM Evaluation board | TI.com In order to start developing the software?
Also what is the process for coding the module? Can it be soldered to the evaluation board even though it is a full module? From my understanding, the CC2564 module should somehow be input the evaluation board so that it can be coded. Any help on this and advice on the process in general would be much appreciated. Thank you.