Other Parts Discussed in Thread: SYSCONFIG
Up to now I could enable it with just 2 defines:
-DGAP_BOND_MGR
- OSAL_SNV=2
Like from the guide below...
1. Configure the stack to include GAPBondMgr functionality by defining the following in build_config.opt
in the stack project:
-DGAP_BOND_MGR
2. The stack must also be configured to use 1 or 2 SNV pages, by defining OSAL_SNV=1
or OSAL_SNV=2
as a preprocessor-defined symbol in the stack project.
In the new sdk_4_40_00_44 it seems to be different. Can someone please point in the right direction?
This is what I get when I call any GAPBondMgr function if I manually define in my app DGAP_BOND_MGR and OSAL_SNV=2