Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1,
Hi everyone,
I have the following scenario, 2x receiving setups (RX) LAUNCHXL-CC26X2R1, each connected with a BOOSTXL-AOA, each running on a separate laptop, using the RTLS_UI.
As the transmitting unit (TX) I have 1x LPSTK-CC1352R, modified with this soffware flashed on it (https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/bluetooth-forum/983980/lpstk-cc1352r-aoa-example-rtls_slave-lpstk-cc1352r?tisearch=e2e-sitesearch&keymatch=LPSTK-CC1352R#)
My question now is: can the LPSTK-CC1352R set up a connection with 2 receiving setups (RX) LAUNCHXL-CC26X2R1 at the same time or can it only handle one at a time? Right now, when I test it, it only connects to one RX unit, and the other one rests, but I would like to have them both connected at the same time. Is there a chance to change something in the software for the LPSTK?
Thanks in advance,
Best regards.