Other Parts Discussed in Thread: CC256XB-BT-SP
Hello,
I have been trying to establish a Bluetooth connection between two sets of dk-tm4c129x with cc2564modaem boards and need to apply the service pack (CC256XB-BT-SP). After changing all of the (5000, 0x00) in the bts file to (5000, any) in the HCItester tool, I am getting the timeout error seen below when I try to execute the script.
16:22:30.115 ERROR - File: "C:\ti\cc256xb_bt_sp_v1.8\CC256XB_BT_SP\v1.8\HCIscript.txt", Line: 22
16:22:30.115 ERROR - Timeout waiting for event HCI_Command_Complete_VS_Update_Uart_HCI_Baudrate_Event
16:22:30.115 ERRORed Line (22): Wait_HCI_Command_Complete_VS_Update_Uart_HCI_Baudrate_Event 5000, any, 0xff36, 0x00
From what I have read in the forums, I need to put my board in transparent mode with some sort of code that I have to write myself? Is this accurate and is there any resources that can help with this? I am relatively inexperienced with this level of coding and any advice would be appreciated.
Thanks,
Jeremiah