This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

How to Build SensorTag(CC2650) inculde OAD service

Prodigy 40 points

Replies: 8

Views: 5214

Hi All,

Location in C:\Program Files (x86)\Texas Instruments\SmartRF Tools\BLE Device Monitor\firmware\cc26xx folder

CC2650SensorTag_BLE_All_v1_20.hex(size:300KB)

The hex file how to build out?Is it use python script(hexmerge.py) merge follow hex file?

BIM_ext.hex(FlashOnly_SensorTag)+SensorTagAppFlashOnlyOAD.hex+SensorTagStackFlashROM.hex

Someone can explain how to do?

Thanks!

  • Guru 104890 points
    Hello,

    Yes, please see the "Working with Hex Files" section in the BLE 2.1 SW Developer's Guide (SWRU393).

    Best wishes

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • In reply to JXS:

    Hi JXS,

    According to the section,This super hex is only APP+STACK hex files.
    BIM_ext hex and super hex download to CC2650STK ,but it is not work.(using android app can't scan the device),than CC2650SensorTag_BLE_All_v1_20.hex download to CC2650STK,it is can run.

    I had built the OADTarget project,The super hex where On-chip OAD is consist of BIM+APP+STACK hex file.

    Download to SmartRF06EB+CC2650EM-7ID,can use OAD program by BLE Device Monitor.

    How to build OADTarget by Off-chip OAD ?

  • Hello,

          I have figured out how to generate workable super hex file (BIM + SensorTag + SensorTagStack) for off-chipet OAD in CCS IDE.

          Modifications:

          1, Import ble/util/BIM_ExtFlash project to CCS, and add below post step:

              "${CG_TOOL_HEX}" -order MS --memwidth=8 --romwidth=8 --intel -o "${ProjName}.hex" "${ProjName}.out"

              Because, by default BIM_ExtFlash project does not generate hex file in CCS, but this step exist in IAR IDE.

          2, Add below merge script in SensorTag project:

             python "C:/Python27/Scripts/hexmerge.py" -o "${PROJECT_LOC}/FlashOnlyOAD/OAD_IMAGE_FULL.hex" -r "000:1FFFF" --overlap=error "${PROJECT_LOC}/FlashOnlyOAD/${ProjName}.hex":0000:1EFFF "${PROJECT_LOC}/../${ProjName}Stack/FlashROM/${ProjName}Stack.hex" "${PROJECT_LOC}/../../../../util/BIM_extflash/CC26xx/CCS/FlashOnly/BIM_ExtFlash.hex":1F000:1FFFF

              Please notice, the sample merge script in OAD document is incorrect, please refer document at http://processors.wiki.ti.com/index.php/CC2650_SensorTag_User's_Guide#Building_SensorTag_SuperHex_File 

    After above modifications, follow below steps to build:

    Step 1: Build BIM_ExtFlash project to generate BIM_ExtFlash.hex

    Step 2: Build SensorTagStack project to generate SensorTagStack.hex

    Step 3: Build SensorTag project to generate SensorTag.hex. And the merge script will combine  BIM_ExtFlash.hex + SensorTagStack.hex + SensorTag.hex togather

    After above build steps, you can use "Flash Programmer 2" to flash super hex file to CC2650 sensor tag device.

    Hope it helpful to you.

  • In reply to Lu, Ken:

    Hi Lu,Ken

    I read your post. I am also trying to generate super hex file for CC2650 Sensortag application.

    But merge script you mentioned in your post, where to add it exactly.

    Mamata N.

  • In reply to Mamata Nivalkar:

    Mamata,

            Add to the post build step. Please see attached picture.

  • In reply to Lu, Ken:

    Great job!
    That works for me too,
    I was unable to build the superhex by following the guidelines in that document processors.wiki.ti.com/.../CC2650_SensorTag_User's_Guide .
    Actually i bricked the device doing what is in there.

    You saved several of my days, much appreciated!

    Pietro
  • In reply to Lu, Ken:

    what is the last part in post-build steps window ?
  • In reply to Lu, Ken:

    Hi Lu,

    When Building the BIM_ExtFlash I am getting several Errors.

    Description Resource Path Location Type
    #137 struct "<unnamed>" has no field "status" bim_main.c /BIM_ExtFlash/Application line 438 C/C++ Problem
    #20 identifier "EFL_ADDR_IMAGE_BLE" is undefined bim_main.c /BIM_ExtFlash/Application line 452 C/C++ Problem
    #20 identifier "EFL_ADDR_IMAGE_APP" is undefined bim_main.c /BIM_ExtFlash/Application line 448 C/C++ Problem
    #20 identifier "EFL_IMAGE_INFO_ADDR_BLE" is undefined bim_main.c /BIM_ExtFlash/Application line 430 C/C++ Problem

    How could I correct this?

    Thanks and Regards,
    Danish

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.