Other Parts Discussed in Thread: CC2564
I've read posts that the TI chips cannot support simultaneous LE and BR/EDR but I was wondering if this is a limitation of the TI chip or if it's a limitation of the BT spec. The BT spec has a feature for simultaneous LE and BR/EDR to the same remote device in Volume 2, Part C, 3.2 Feature Definitions:
"This feature indicates that the Host supports simultaneous LE and
BR/EDR links to the same remote device.
This bit shall only be set if the Simultaneous LE and BR/EDR to
Same Device Capable (Controller) bit is set on the local Controller.
The local Host sets this feature bit to indicate to a remote device that
the local device is capable of supporting simultaneous LE and BR/
EDR connections to the peer device.
A remote Host uses this feature to determine whether simultaneous
LE and BR/EDR connections are possible to the peer device."
If the BT spec allows this, does anyone know of a chip that supports this feature?