HI,
I'm testing the HRP connection in the following configuration:
- EKS-LM4F232 board
- CC256x Stellaris Bluetopia SDK v1.0 HRPDemo NoOS
- Evaluation Module TIwi uB2 configured to use Internal SlowClock
- Polar H7 sensor
I'm able to connect to the sensor issuing the following command sequence:
"CONNECTLE 0022d0259f6c"
"DISCOVERHRS 1"
"ConfigureRemoteHRS 1"
Then I start to receive data correctly.
Then randomly the sensor disconnect. Sometimes after few seconds sometimes after 1-2 minutes.
The message I receive is:
Server>
etGATT_Connection_Device_Disconnection with size 12:
Connection ID: 95.
Connection Type: LE.
Remote Device: 0x0022d0259f6c.
Server>etLE_Disconnection_Complete with size 9.
Status: 0x00.
Reason: 0x3b.
BD_ADDR: 0x0022d0259f6c.
There is something I can do?
Kind Regards
Andrea