Hi,
Can BLE advertise while being connected ?
If it’s not, can this be implemented ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can BLE advertise while being connected ?
If it’s not, can this be implemented ?
Thanks
Combo roles allow you to advertise while connected. The advertisements will be non-connectible.
BR
Greg
A peripheral can't connect to more that one device, but it can still send out non-connectable advertisements. The basic SimpleBlePeripheral demo allows this, Just start a non-connectable advertisement when you get connection established event.
There are some combo role examples here.
http://processors.wiki.ti.com/index.php/CC254X_Embedded_Examples
The peripheral broadcaster example is prob out of date, but the 1.4 stack peripheral role profile supports it (so no need for peripheral broadcaster).
TI central will connect to multiple devices, and can be a central and a broadcaster.
BR,
-Greg