This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 786
Hello,
does TI plan to make it possible to directly buy the assembled form of the module TIDC-BLUETOOTH-LOW-ENERGY-LONG-RANGE?
I would like to evaluate the performance of this design (we have a simple lab for simple RF measurements), before I possibly place an order to our HW development vendor to try to integrate this module into our application. Unfortunately, I cannot ask that company to build just 2 or 3 such modules and for a higher amount of them I simply do not have a budget :-(
Thank you in advance for your help or advice :-)
Kind regards,
Tom
------------------------------------------------
http://crypto.hyperlink.cz
That module is not available for sale, but you can download the design files & provide to your CM. An alternative solution may be the BLE121LR module from BlueGiga: www.bluegiga.com/.../ble121lr-bluetooth-smart-long
Best wishes
Please click the "This Resolved My Issue" button on this post if it answers your question
In reply to JXS:
In reply to Tomas Rosa:
If my post answers your question, please click on "This Resolved my issue" button to benefit others who have the same issue.
YK Chen
Build OpenThread Sleepy End Device doorlock prototype to test with Rasperry Pi OpenThread Border Router
How to use two UARTs in CC26x2 and CC13x2
SwitchBot DIY using LPSTK-CC1352R , SG90 servo motor, and ProjectZero to away from COVID-19.
How to use two endpoints in SIMPLELINK-CC13X2-26X2-SDK Z-Stack.
CC13xx TRX WOR project.
How to create a periodic event to toggle BLE Advertising in CC26xx simple_peripheral example
How to use indication in simple_peripheral example and use Btool to enable indication
How to check APS ack in TI Z-Stack
How to detect button hold in CC26x2, CC13x0, CC13x2 SDK.
660 Zigbee devices in the same Zigbee network!
In reply to YiKai Chen:
Excellent ;-)
As I am also searching for an affordable extended range sniffer (for security tests / demonstrations), I would like to also use the BLE121LR with your SmartRF Packet Sniffer. (of course, there is the awesome Ubertooth, but let's say this is a bit different sort of device) Now, the manual mentions only the CC2540 USB dongle is supported. On the other hand, the PC-part of this tool apparently supports other chips connected through the CC debugger. Is there a fw for CC2541 to work with the sniffer?
As I know, there is no specific sniffer FW for CC2541. However, there is a FW sniffer_fw_cc2540_uart.hex for SmartRF05EB with CC2540EM. I think this FW should be workable on CC2541 so you can try it. You can find sniffer_fw_cc2540_uart.hex under C:\Program Files (x86)\Texas Instruments\SmartRF Tools\Packet Sniffer\bin\general\firmware if you install TI Packet Sniffer.