Hi all,
I have gone through different post in this forum discussing about enabling automatic parameter update request when a connection is formed. So many posts discusses that we can update the connection parameters during the process as required. For my application i need to update different connection interval based on requirement for saving power consumption.
A discussed by Svendbt in 
"Android versions <5 does not allow you to request other connection intervals (it ignores preferred intervals by the peripheral).".
1)I need confirmation for this that if i try to update the connection related parameters during the process then it will not update in mobile phones with android version < 5. My android application will support in mobile phones version >4.4.
Will "GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );" API have no effect for android versions < 5?
2)Is there any concern for connection interval assigned by central device for different mobile phones? I have set
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 8(10msec)
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 12(15msec)
So my question is will different mobile phones connect to my BLE peripheral device within above set connection interval(or even > 7.5ms)? I have tested in different mobile phones but in some phones there is no problem in receiving data when i send 80bytes data with 25msec interval but in other phones too many data get missed. Is this issue caused due to low connection timing range set and withing this range central device would not connect?
Thanks