Hi,
I am trying to connect CC3200 to CC265 using SPI connection and running 2650 as a central device . Would host test project would satisfy the needs for the task ?
If so what modification would be required to do so.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The CC2650D_4XS.h file only contains references to SPI0, are you certain that the 4x4 chip supports SPI1?
The npi_config.h file contains "error "NPI ERROR: Board_SPI1 SPI module must be used for NPI."" - Is this true, that you must use SPI1 instead of SPI0?