Hi all, I just got my CC2650 LaunchPad rev 1.1.
I was wondering if there was any documentation for this platform other than .
I am looking to build a project with the CC2650 and would like to get started with at least some board files. It would be great if TI released the source code for the demo application as I suppose it already has all the drivers and examples to access the peripherals on the board. (serial flash, buttons, leds)
The schematic for the LaunchPad rev 1.1 would also be useful in order to implement a basic custom PCB design with the same configuration.
I would like to add that I was surprised to receive a LaunchPad which is not exactly the same as the image on the store. I first thought I wouldn't be able to program the SensorTag with the LaunchPad debugger as the 5x2 pin connector is different to the one on the store image. I then found this wiki page which makes it clear it is possible with the same cable/connector.
Thanks!