This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program a new CC2640 device via UART/SPI using ROM bootloader

Other Parts Discussed in Thread: CC2640

Hi,

We are planning to make a custom board with CC2640 device. We have a few doubts regarding downloading firmware to the device for the first time

1) Is JTAG needed on the custom board? Can't we download the firmware using UART/SPI even for the first time?

2) If yes, are there any hazards (device gets locked , etc. ) if we use only UART/SPI for flashing the device?

3) Can we modify the Customer configuration area (CCFG) even before firmware download ? So that I can configure a GPIO pin for the backdoor 

Waiting for your reply,

Thank you,

Surya.