Other Parts Discussed in Thread: CC2541
Hi,
We are designing a board with the CC2541 device and ST microcontroller which we want to control the system.
We wish to design the board without the CC debugger connector and configure the CC2541 with the I2C interface using the ST microcontroller. In other words, the CC2541 only connection is the I2C to the microcontroller, ST is the master and CC2541 is the slave.
Is it possible to configure the CC2541 device via I2C on power up? I saw on the userguide that the default I2C state is to be disabled.
Please advise me if it it possible or what else could fit.
Thank you,
Doron