So perhaps I just do not understand the api calls to the functions in halflash or nvocop but I really could use a small example these being used in a task...
Say for instance that I wanted to Write to memory of size int8_t about 4096 times....
Could I use a basic for loop with the value being hit by 8 to call the read and write from a given memory location?
An ideal case for my use would be to have a total of int8_t x [8192] different entries without using an array (I get ram issues if I do this...)I am unsure which direction I should go for the size of information I would like to use in my application (halflash vs nvocop)
Also if you happen to suggest a direction do you have a basic example of the function being used in both a read and a write of a int8_t value into flash....
If this is a tad to vague I can elaborate on what I have tried and failed on thus far....