HI,
I want to transmit around 2000 bytes in order to check the maximum throughput that this board will allow to trasmit but in order to do so I have to send data that is big enough to fill the whole frame in Bluetooth. I am using a simple application in Java which allows me to transmit sample message to the board and back, then I measure the duration of the process and I have the maximum throughput that can be achieved. On the board side I am using Spp demo, how can I change the MTU value in L2CAP so I can send bigger size data at once?
thanks for your help