We are currently performing a design review and I have found our CM has used a CC2564 as the BT module within a component to be placed in conditions that will exceed the maximum operating temperature of 85°C. The maximum temperature which can be reached is between 105 and 115°C. Can anyone please tell me if there is any room for this temperature rise, what are the consequences for operating in short durations above the maximum operating temeperature? Is there a chip compatiable to the CC2564 which can support these higher temperatures? Any information will be greatly appreciated.
Thanks,
Jessie