Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640, CC2650
In the 4.2 Bluetooth specification, it states
"The Link Layer shall use one of two possible clock accuracies. During a connection event or advertising event the Link Layer shall use the active clock accuracy; otherwise it shall use the sleep clock accuracy."
When advertising, I assume the CC2640R2F works fine using the 24-MHz Crystal. After a connection is established, if I do not have the 32.768-kHz Crystal installed, CC2640R2F will not output a signal.
Why is it that if I do not have the 32.768-kHz Crystal installed, CC2640R2F will not output a signal?