Tool/software: TI-RTOS
Hi, sir
I met a strange problem today: when I change the value of 'm3Hwi.nvicCCR.UNALIGN_TRP' from 0 to 1 in app_ble.cfg of example multi_role which comes with simplelink_cc2640r2_sdk_1_30_00_25, this demo will hang.
I even could not pause the iar since iar would either crash or run into unresponsive status and I must kill the progress manually.
However, when I change the value of 'm3Hwi.nvicCCR.UNALIGN_TRP' back to 0, every thing goes well.
Can anyone tell me what is wrong about this param?
PS: I notice a warning in linking stage that iar complains:
Warning[Lt009]: Inconsistent wchar_t size
CryptoCC26XX.orm3(drivers_cc26x0r2.arm3) and 66 other objects have wchar_t size 16 bits
ble_user_config.o and 57 other objects have wchar_t size 32 bits
I do not know if this is the root cause?