This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640R2F: Connecting issue, after porting project with cc2650 to cc2640r2f

Part Number: CC2640R2F

Tool/software: TI-RTOS

I'm porting our project (based on project_zero) and now I have problems with connecting to our device. 

Log from device below:

#000071 [ 315.307 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:729) Connected. Peer address: 0x57C8EB8F1C3B
#000072 [ 315.511 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:954) HCI Command Complete Event received
#000073 [ 319.905 ] ERROR: (../Application/Eseal/Source/WirelessConnectionTask.c:1008) Flow control violated. Opcode of offending ATT msg: 0x10
#000074 [ 327.226 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:954) HCI Command Complete Event received
#000075 [ 327.234 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:1129) (CB) GAP State change: 4, Sending msg to app.
#000076 [ 327.234 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:1129) (CB) GAP State change: 2, Sending msg to app.
#000077 [ 327.234 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:759) Disconnected / Idle
#000078 [ 327.235 ] INFO: (../Application/Eseal/Source/WirelessConnectionTask.c:688) Advertising

I have absolutely no idea how I should debug it. Can anyone give me advice?