Hello
I am trying to use BTool for the first.
I am using LaunchXL-CC2650 with multi role project on it. The project works (if I put aside all the other problems I encounter with it ...).
When I try to connect to BTool I get this error:
"GAP device initialization timeout. Device may not function properly"
But the device is fine. What could be the problem?
And what port should I connect it to, the class auxilliary data port or the class application/user UART? I've tried both and none worked.
I have seen posts about this problem but they had no answer ..
Thanks
Amit