This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

One minute to understand BLE MTU data package

1.Profile
  * MTU: ATT Maximum Transmission Unit (MTU) is the maximum length of an ATT packet. The ATT MTU is defined by the L2CAP and can be 
anywhere between 23 and infinity. The implementation of the Bluetooth stack is the key factor of determining the ATT MTU on both client and peripheral.
     A generic ATT packet has the following structure:










    MTU exchange happens after master and slave device build up connection, refer: "One minute to understand BLE connection data package"

http://www.viewtool.com/forum/vi ... &extra=page%3D1

  Below is the comparison of few of major wireless protocol (units: bytes)
  ****************************************************************      
  Ethernet:1500
  IEEE 802.3/802.2: 1492
  X.25: 576
  BLE: 23 (for BLE4.0/4.1), 251 (for BLE4.2) => that's why wifi could be used to transfer video,traditional bluetooth(BT) could be used to transfer audio, and BLE only could be used to transfer control data.
  ****************************************************************
  * MTU exchange command: is ATT command
  * MTU exchange procedure see below:





  * MTU tow commands(“MTU request”and“MTU response”)description in detail(see“4”)

2.Keyword: Hollong BLE Sniffer, BLE Data Analyzer,BLE Data Capture

3.Preparation before capturing BLE data 
  * Hardware:One BLE device (as slave device) and one master device(such as lightblue or redwoods app in iOS or Android);
           One HOLLONG BLE SNIFFER 
  * Software:Hollong BLE sniffer and protocol analyzer
        download link:

http://www.viewtool.com/index.ph ... hollong-4-0-4-1-ble

4. MTU REQEUST
   Complete data (marked by blue color)






    1) Access Address: 0xaf9a8c69
    Fixed 4 bytes,specified by CONNECT_REQ(see:http://www.viewtool.com/forum/vi ... &extra=page%3D1




   2) Header Info
 Data Header: 0x0706    000. .... = RFU: 0
    ...0 .... = More Data: False
    .... 0... = Sequence Number: 0
    .... .1.. = Next Expected Sequence Number: 1
    .... ..10 = LLID: Start of an L2CAP message or a complete L2CAP message with no fragmentation (0x2)
    000. .... = RFU: 0
    ...0 0111 = Length: 7






 3) L2CAP Length
    In BLE protocol layer,All of GAP,GATT and SMP use L2CAP channel to transfer command to LINK LAYER,L2CAP packing need to specify 
L2CAP length and channel ID
    Length: 3






   4) L2CAP CID:channel ID
   CID: Attribute Protocol (0x0004)






    5) ATT command
     standard:    




     actual data package:
    Opcode: Exchange MTU Request (0x02)
    0... .... = Authentication Signature: False
    .0.. .... = Command: False
    ..00 0010 = Method: Exchange MTU Request (0x02)







   6) MTU value (requested)
    Client Rx MTU: 185







   7) CRC 






5. MTU RESPONSE
    completed data package:






    1) Access Address: 0xaf9a8c69
    Fixed 4 bytes,specified by CONNECT_REQ(see:http://www.viewtool.com/forum/vi ... &extra=page%3D1




   2) Header Info
 Data Header: 0x0706    000. .... = RFU: 0
    ...0 .... = More Data: False
    .... 0... = Sequence Number: 0
    .... .1.. = Next Expected Sequence Number: 1
    .... ..10 = LLID: Start of an L2CAP message or a complete L2CAP message with no fragmentation (0x2)
    000. .... = RFU: 0
    ...0 0111 = Length: 7






    3). L2CAP length
        same as MTU request.
        Length: 3






    4).L2CAP CID: channel ID
        same as MTU request.
       CID: Attribute Protocol (0x0004)






    5). ATT command
       standard:






       For this example:
       Opcode: Exchange MTU Response (0x03)    0... .... = Authentication Signature: False
    .0.. .... = Command: False
    ..00 0011 = Method: Exchange MTU Response (0x03)






     6) MTU value
      Server Rx MTU: 23






      7)CRC
       CRC: 0xf4767e
    [Expert Info (Note/Checksum): CRC unchecked, not all data available]