Other Parts Discussed in Thread: CC2540, BLE-STACK
Is 3 minutes the expected amount of time for the Over-the-Air Download (OAD) code to send ~100K of code? I'm using a SmartRF05 eval board with a CC2540 daughter board running the OADManager app and connecting to a CC2541-based module.
If this is the "normal" speed, it may end up being a show-stopper for us.
Are there any tricks or suggestions people can offer to help speed this up? Ideally by a factor of 10 or more.
I realize I sound a little nitpicky - but Bluetooth routinely sends data at a much faster overall rate than this - so OAD must be doing something "weird" to make it that slow. Especially considering the comment in section 14.3 of the OAD manual about OAD being designed "to reduce code size and increase data throughput as much as possible."
Thanks.