Part Number: CC2564B
SPP Server
SPPClient
Hi,
I'm using SPPLE Demo with MSP430.
I want to connect multiple SPP at the same time, but there is some problem with connect on client.
at the top of this thread, i post screenshot of my tera term.
When execute [openserver] command on Server and execute [openremoteserver] command immediately on Client,
connection error occurs with a very high probability like screenshot.
It seems to connected successfully, but it does not. Just output open confirm message.
biggest problem is the waiting time to connect SPP is too random.
sometimes it can connect immediately, but sometimes it can connect 7~10 seconds left.
1) Is there any way to reduce waiting time to connect?
2) Or can I increase connection timeout on client?
Best regards,
DW