This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIDC-BLE-TO-WIFI-IOT-GATEWAY: Need of Extrenal flash in IoT Gateway

Prodigy 115 points

Replies: 1

Views: 417

Part Number: TIDC-BLE-TO-WIFI-IOT-GATEWAY

Why there are two external flash required, one for each processor (i.e. cc3200 and cc2650) in a gateway ? 

  • External flash are usually used for OTA downloads so that firmware can be updated reliably over-the-air without compromising application image size. You'd want to be able to do this for both processors.

    Regards,
    Katie

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.