Part Number: SIMPLELINK-CC2640R2-SDK
Other Parts Discussed in Thread: CC2640R2F
Hi,
i am using SableX R2 on a custom board with CC2640R2 chip 5x5 on it. I am using the latest SDK_1_50_00_58.
I have noticed that once the watchdog has fired and reset was set to on, the device dont reset and stays in an unkown state.
I have also to disable reset and set a watchdog callback function to hard reset the software if its fired.
This function is never called even if i uncomment "watchdog_clear(...)". (debug/jtag not attached)
To make the watchdog fire the interrupt to go to the callback function, i have to add a "while(1){};" loop in my task.
Then i can see that every time it enters the callback function it turns the LED on and reset the controller.
But if i dont have the while loop, the function gets never called.
Any idea?
void iniWatchDog(void)
{
Watchdog_Params params;
/* Call board init functions */
Watchdog_init();
/* Create and enable a Watchdog with resets disabled */
Watchdog_Params_init(¶ms);
params.callbackFxn = (Watchdog_Callback)watchdogCallback;
params.resetMode = Watchdog_RESET_OFF;
//params.debugStallMode = Watchdog_DEBUG_STALL_ON;
watchdogHandle = Watchdog_open(Board_WATCHDOG0, ¶ms);
// if(watchdogHandle!=NULL)
// Watchdog_setReload(watchdogHandle, Watchdog_convertMsToTicks(watchdogHandle,10000));//90000 mseconds
}
/*
* ======== watchdogCallback ========
* Watchdog interrupt callback function.
*/
void watchdogCallback(uintptr_t unused)
{
/* Clear watchdog interrupt flag */
Watchdog_clear(watchdogHandle);
/* Insert timeout handling code here. */
PIN_setOutputValue(hGpioPin,CC2640R2_LAUNCHXL_PIN_GLED,0);
delay_ms(5000);
//HAL_SYSTEM_RESET();
SysCtrlSystemReset() ;
}