Other Parts Discussed in Thread: CC2650, TIDC-CC2650-CC2592-EMK, , CC2592
Hi,
Using the TIDC-CC2650-CC2592-EMK as reference, we replace the CC2650 with CC2640R2F and had the PCB board done. At the board file I need to set the RF Front End and Bias configuration define. Since I used the Simple Peripheral the define is set below for Differential RF and internal biasing (default for CC2640R2 LaunchPad). But reviewing the schematic diagram It seems more like Single-Ended RF. What define should I set at the board file?
/*
* ============================================================================
* RF Front End and Bias configuration symbols for TI reference designs and
* kits. This symbol sets the RF Front End configuration in ble_user_config.h
* and selects the appropriate PA table in ble_user_config.c.
* Other configurations can be used by editing these files.
*
* Define only one symbol:
* CC2650EM_7ID - Differential RF and internal biasing
(default for CC2640R2 LaunchPad)
* CC2650EM_5XD – Differential RF and external biasing
* CC2650EM_4XS – Single-ended RF on RF-P and external biasing
* CC2640R2DK_CXS - WCSP: Single-ended RF on RF-N and external biasing
* (Note that the WCSP is only tested and characterized for
* single ended configuration, and it has a WCSP-specific
* PA table)
*
* Note: CC2650EM_xxx reference designs apply to all CC26xx devices.
* ==========================================================================
*/
#define CC2650EM_7ID
-kel