Hi all,
In order to use CC2540 USB Dongle (I have rev. 1.0.1) it was recommended in another thread to install SmarRF studio to get USB driver Windows 10 x64.
I did USB trace on Win 10 and this device: USB device descriptor clearly states USB VID and PID:
- idVendor Texas Instruments 0x0451
- idProduct 0x16AA
In Setup_SmartRF_Studio_7-2.10.0.exe cebal driver has the following USB PIDs:
cebal2_x64.inf
;******************************************************************************
; Models section (specifies the supported device's hardware ID)
;------------------------------------------------------------------------------
; x64-based systems
[_Models.ntamd64]
%S_DeviceDesc1% = _Install_1, USB\VID_11A0&PID_DB20 ; CC2430DB
%S_DeviceDesc2% = _Install_2, USB\VID_11A0&PID_EB20 ; SmartRF04EB
%S_DeviceDesc3% = _Install_3, USB\VID_0451&PID_16A0 ; SmartRF05EB
%S_DeviceDesc4% = _Install_4, USB\VID_0451&PID_16A2 ; CC Debugger
%S_DeviceDesc5% = _Install_5, USB\VID_0451&PID_16AB ; CC2511 USB dongle
%S_DeviceDesc6% = _Install_6, USB\VID_0451&PID_16AC ; CC2511 USB nano dongle
%S_DeviceDesc7% = _Install_7, USB\VID_0451&PID_16AD ; CC1111 USB dongle
%S_DeviceDesc8% = _Install_8, USB\VID_0451&PID_16AE ; CC2531 USB dongle
%S_DeviceDesc9% = _Install_9, USB\VID_0451&PID_16B2 ; Generic CCxxxx USB dongle
%S_DeviceDesc10% = _Install_10, USB\VID_0451&PID_16B3 ; CC2540 USB dongle
%S_DeviceDesc11% = _Install_11, USB\VID_0451&PID_16B5 ; SmartRFTrxEB
%S_DeviceDesc12% = _Install_12, USB\VID_0451&PID_16B8 ; Generic CCxxxx evaluation board
%S_DeviceDesc13% = _Install_13, USB\VID_0451&PID_16C6 ; CC2544 USB dongle
%S_DeviceDesc14% = _Install_14, USB\VID_0451&PID_16CB ; CC2538EM
It is obvious that no driver could be found for such cc2540 dongle with PID 0x16AA.
Could anyone at TI explain