Part Number: CC2564C
Hello,
I have a question regarding TI bluetooth chip CC2564C. I'm using it in combination with STM3240G-eval board (CC256x STM32 Bluetopia SDK v4.2.1.0)
I've tried to change output power within HFP_AG sample demo: HCI_VS_DRPb_Set_Class2_Single_Power.
However, with the spectrum analyzer I cannot see any difference between standard settings and custom settings (-50 dBm).
I added the following code :
int InitializeApplication(HCI_DriverInformation_t *HCI_DriverInformation, BTPS_Initialization_t *BTPS_Initialization)
{
int ret_val = APPLICATION_ERROR_UNABLE_TO_OPEN_STACK;
/* Next, makes sure that the Driver Information passed appears to be */
/* semi-valid. */
if((HCI_DriverInformation) && (BTPS_Initialization))
{
/* Try to Open the stack and check if it was successful. */
if(!OpenStack(HCI_DriverInformation, BTPS_Initialization))
{
/* Lower Output Power */
ret_val = VS_Set_Max_Output_Power(BluetoothStackID, 0);
if(!ret_val)
{
Display(("\r\n VS_Set_Max_Output_Power success \r\n"));
}
else
{
Display(("\r\n VS_Set_Max_Output_Power fail %d \r\n", ret_val));
}
/*... rest of the InitializeApplication */
....
}
I can see the command executed with TI HCI Logger:
Default settings for TX output power (limited in software to 10 dBm):
Set TX output power to -50 dBm - no impact on TX output power (measured with spectrum analyzer)
Does anybody have an idea why I see no difference with the spectrum analyzer regarding the TX output power?
Thanks and Regards
Tim