This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2650: How to set ADC input to IDIO8 with CC2650 RHB package?

Part Number: CC2650


Tool/software: TI-RTOS

Hello,

I need read adc data from DIO8.of CC2650 in RHB package. DIO8 can be set to either digital or analog.

I started with the CC2650 launchpad ADC example project and it works well with both adc channels: 

#define Board_ADC0 CC2650_LAUNCHXL_ADCVSS
#define Board_ADC1 CC2650_LAUNCHXL_ADCVDDS

Now I need re- wire ADC1 to DIO8

1: in Board.h, I change the definition:

#define Board_ADC0 CC2650_LAUNCHXL_ADCVDDS
#define Board_ADC1 CC2650_LAUNCHXL_ADC0     // IOID_8

2: in cc2650_launchxl.h 

#define Board_DIO8_ANALOG          IOID_8

3: cc2650_launchxl.c lookup table, change to IDOI8

const ADCBufCC26XX_AdcChannelLutEntry ADCBufCC26XX_adcChannelLut[] = {
{PIN_UNASSIGNED, ADC_COMPB_IN_VDDS},
{PIN_UNASSIGNED, ADC_COMPB_IN_DCOUPL},
{PIN_UNASSIGNED, ADC_COMPB_IN_VSS},

                        // {Board_DIO23_ANALOG, ADC_COMPB_IN_AUXIO7},
{Board_DIO8_ANALOG, ADC_COMPB_IN_AUXIO7},

4: in hardware attributes, modify the first config accordingly:

const ADCCC26XX_HWAttrs adcCC26xxHWAttrs[CC2650_LAUNCHXL_ADCCOUNT] = {
{
.adcDIO = Board_DIO8_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO7,
.refSource = ADCCC26XX_VDDS_REFERENCE, // ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL

5: set pintable:

const PIN_Config BoardGpioInitTable[] = {

Board_RLED | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, /* LED initially off */
Board_GLED | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, /* LED initially off */
Board_BTN1 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_BOTHEDGES | PIN_HYSTERESIS, /* Button is active low */
Board_BTN2 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_BOTHEDGES | PIN_HYSTERESIS, /* Button is active low */

Board_PwrEnb | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX, // Enable regulator

Board_DIO8_ANALOG | PIN_INPUT_DIS|PIN_GPIO_OUTPUT_DIS,        // I tried enable, disable, or ignore, no difference

However, I even couldn't get stable reading no matter I tie IDIO8 to Vcc or GND:

Did I miss any steps?

Thanks for help!

PJ