Tool/software: Code Composer Studio
Hello.
Im trying to run the ble5_simple_central_cc2640r2lp_app code on the CC2652R1 launchpad using CCSv8.
The code compiles, but when loading it, i get the error :
Cortex_M3_0: Target timed out! (Block 1)
Cortex_M3_0: Status 0x0102: Target flashloader failed to erase sector 1. Low level function returned status 3 (Incorrect parameter value).
Cortex_M3_0: Command=4 -- addr=0x00002000 -- length=0x00001000
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: C:\Users\AlfiNuc\workspace_v8_cc26x2r1\ble5_simple_central_cc2640r2lp_app\FlashROM_StackLibrary\ble5_simple_central_cc2640r2lp_app.out: Load failed.
This might be because i used the target configuration file that was provided in the example code.
When i use the correct target configuration file (for example from project_zero demo), then the code gets loaded without this error, but there is nothing in the serial terminal window. That makes me think the code is not running properly. As i uderstand it is supposed to create a menu structure to the serial terminal. I have successfully used the serial terminal in project_zero example, i assume it has the same parameters in simple_central example
How to properly port this simple_central example to the CC26X2R1 launchpad?